Part Number: MSP430F2618
Greetings.
I wish to use the low frequency crystal oscillator LFXT1 / ACLK as the source for main processor clock MCLK.
The processor defaults to Digitally controlled Oscillator DCO at start up, and I will code the change to…
Abdel said: CODEGEN-1476: EXT_EP-8121:
For more context, here is the forum thread which resulted in this entry being filed. It can only occur in hand-coded assembly. Since ...
Abdel said: we do not utilize assembler code
... you can ignore it.
Abdel said…
Part Number: MSP430F2618 I'm attempting to understand the behavior of the compiler when executing the CLRX(.B,.A) dst command on the MSP430F2618 microcontroller (uC). Specifically, I'm trying to grasp the addressing mode for extended instructions…
Part Number: MSP430F2618 Greetings.
We have a data logger based on the MSP430Fx2xx processor using a GSM modem for remote access.
Our GSM code is old 2.5G with GPRS. We are upgrading to 4G. The 4G modem uses the AT command set.
We connect to remote servers…
Part Number: MSP430F2618
Greetings.
Our MSP430 program includes a bootloader which I have written.
I would like to use the built in BSL, but I haven't access to the BSL pins P1.0 and P1.1 They are used for other things.
Is it possible to access the…
Part Number: MSP430F2618 HI,
There is foreign matter in MSP430F2618TGQWTEP chip. Please help to analyze the reason. The customer wants to know about the relevant quality inspection. Thanks!
Part Number: MSP430F2618 We have received an MSP430F2618TGQWTEP package from a distributor with part markings that do not seem to match the ones mentioned in TI's documentation.
Could this possibly be an older revision with different markings?
This…
Part Number: MSP430F2618 The datasheet doesn't seem to specify what the part markings are for MSP430F2618TGQWTEP, it's highly unlikely that this microcontroller comes without any markings.
I found two websites of unknown reliability that indicate…
Part Number: MSP430F2618 Other Parts Discussed in Thread: MSP-TS430PM64A , MSP-FET , MSP430F4152 Hello,
I am using the MSP430F2618 with the MSP-TS430PM64A dev board and MSP-FET. When I attempt to program the part, it gives the error: "MSP430: Error connecting…