I am using the MSP-GANG430 currently. I brought the MSP-GANG to replace it. I am trying to program the MSP430F415. The programmer MSP-GANG goes and displays it has programmed the chip but when it verify.
Greetings and thanks, (Mel, Jens, Jace )
I have been wrestling with a nearly identical issue on a board based on a MSP430F415; random erasures of one or both flash INFO memory blocks in the field especially on units that are powered up and down at…
Other Parts Discussed in Thread: MSP430F4152 , MSP430F415 Is it possible to program MSP430F4152 with MSP-PRGS430 serial programmer?
It seems possible for MSP430F415 but it's not possible to select MSP430F4152.
Is it necessary to update the driver…
Other Parts Discussed in Thread: MSP430F415 I'm building and executing code for the MSP430F415 processor using CCSv4 with the MSP-FET430UIF JTAG debugger. In the initialization code prior to entering the main() loop, I have a few memset() calls to clear…
Other Parts Discussed in Thread: MSP430F415 , MSP430F4152 I need an extra UART on the MSP430F4152, so I'm using the Timer UART example code from the MSP430F415 to get started. The code works when I try it on the default ports, P1.0 / TA0.0 for TXD and…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…