Part Number: MSP430F447 Hi Team, we would like to confirm if we already used 2 UART of the CPU, can we still add SPI peripheral as an upgrade?
Thanks!
-Mark
Part Number: MSP430F447 Other Parts Discussed in Thread: THS1206 , TMS320C6201 , , ADS8342 , TM4C123FH6PM
Hello,
I received the MCU MSP430 Vs ADC THS1206 EVM source code from the ADC forum at the address below.
https:// e2e.ti.com/support/data-converters…
Part Number: MSP430F447 Tool/software: Code Composer Studio hi
So far i have been using IAR but my code size has crossed 8k so can u suggest me some open source tool so that i can run my code
Part Number: MSP430F447 hi
i have used port pin to enable the motor and using through beam ir sensor i am stoping the motor
problem is in the below code first time its working properly second time the motor stops its not coming out of the while
the code…
Part Number: MSP430F447 Other Parts Discussed in Thread: MSP-EXP430FR5994 hi
i want to access microsdcard which has bmp files . i want to display that in tft . do you have any sample code for that
with regards
senthil
Part Number: MSP430F447 Other Parts Discussed in Thread: L293 Hi
I am driving L293 Ic from Microcontroller.
while programming in Jtag i mean when my board is power on while flashing the code all the port pin connected to motor driver is high and makes…
Part Number: MSP430F447 Hi
i have drawn schematic and i have some unused pin should i have to connect to ground or to pull up , by doing so can i use it later if i want .
regards
senthil
Part Number: MSP430F447 hi
I am planning to interface I2C eeprom to microcontroller msp430f447 .I want to know how to design schematics.Because i don find SDA,SCL pins in the pindetails but the datasheet shows u can interface I2c devices to this processor…
Part Number: MSP430F447 Hi
i am planning to interface 2.4 tft lcd of driver(il9341) of mcufriend to msp430 . pls do share the flow of it bcoz i am not getting any datasheet and proper code for interfacing to lcd
with regards
senthil
Part Number: MSP430F447
Hello.
I am facing following FLL problem in MSP430F447.
However I'm using FLL, DCO frequency is not stable.
For example, when changing the temperature from 25 ° C to -10 ° C, the DCO clock frequency on which FLL is operating…