Part Number: MSP430F47127 I am making a energy meter/reference meter with 0.1 class accuracy based on MSP430F47127.
All thing is ok, but i am not able to provide pulse output for its accuracy check. Although i have provided 1600 impulse/Kwh output through…
Other Parts Discussed in Thread: MSP430F47127 Hi,
I am producing my ac static energy meters based on MSP430F47127 for 3phase 4 wire network. Out of 100 meters 2-3 meters are stuck in field conditions. When we analysed these meters, we found that LF crystal…
Sir,
I am using fft routine for harmonics measurement for a 3 phase supply. And for that i use some calulations that require floating point values not the fft porgrams.
I first developed this code on a msp430f47127 using CCE. I changed my MCU to msp430f47177…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
Aravind, The two microcontroller products that are included in the launchpad are these: * MSP430G2211IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT, BOR, Comparator A+ * MSP430G2231IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer,…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…