Part Number: MSP430F5131 Other Parts Discussed in Thread: MSP430F5132
Hi Experts!
I tried to build any ADC example code for the MSP430F5131. The code example I want to use is MSP430F51x2_ADC10_07.c
However, this is a problem with all ADC10 example codes…
Part Number: MSP430F5131
According to slau208q 7.3.3, "interrupts are automatically disabled during any flash operation". My understanding from reading slau208q is that this is facilitated by the flash memory controller always returning the 0x3FFF (JMP…
Part Number: MSP430F5131 Our customer needs inputs as below-
We are looking for msp430 part number which supports BSL in I2C mode. According to the doc “ SLAU319X–July 2010–Revised April 2019”
MSP430™ Flash Devices Bootloader (BSL…
Part Number: MSP430F5131 Hi MSP430 Expert,
I want to generate two 400khz clock with 180° phase shift by MSP430, high volatge of the clock is 5V, low voltage is 0V. could you please recommend a device and give me code tutorial ?
Kevin
Part Number: MSP430F5131 Tool/software: TI C/C++ Compiler I still struggle with seldom-used C "logical" statements -
for speed faster than using an ISR, I want to spin on an interrupt flag for port P1.2 until it becomes a "1"
What…
Part Number: MSP430F5131 Other Parts Discussed in Thread: MSP-FET I'm using MSP430F5131
i wrote a code in IAR Embedded Workbench,
once i try to download the program i get an error message :
Mon Apr 30, 2018 12:48:56: Fatal error: Could not find device…
Part Number: MSP430F5131 Other Parts Discussed in Thread: MSP-FET , Hello ,
once i try downloading the program to the MCU (by clicking on debug and download button) i get the error :
i think i connected the MSP-FET emulator correctly to the MSP430.
Part Number: MSP430F5131 Tool/software: TI C/C++ Compiler Hello ,
I'm using IAR embedded workbench and compiled my code without any errors , although when i click on download and debug button i get this error (in red):
It looks like the wiring schematic you're referencing is for MSP430F2xx, MSP430G2xx, and MSP430F4xx devices. A more up-to-date schematic can be found in our MSP430 Hardware Tool's User's Guide Figure 2-3:
You've mentioned this board was being…
Part Number: MSP430F5131
Tool/software: TI C/C++ Compiler
Hello ,
I'm new to this field of microcontroller and i need you quick help with a new project of mine.
I'm using MSP430F5131.
I will explain a little about the project :
My main goal…