I just checked Olimex website and I realized that MSP430F5244 is not listed in the supported device of the MSP430-JTAG-TINY-V2 JTAG, which I use.
Here is the list - www.olimex.com/.../tiny-v2-supported-mcus.txt
Do you know is the MSP430G2 value…
Hi John, Thank you for the very detailed information - it is really helpful and rules out some common issues. I noted that you mentioned that your version for the firmware inside the MSP-GANG430 itself is The GANG430 is "GANG430-153.TXT Version 1.53"…
Other Parts Discussed in Thread: MSP430F5249 , MSP430F5529 , MSP430F5244 , MSP-TS430RGC64C Hi,
I'm debugging with MSP430F5249.
I have a question about breakpoint.
1. Set a breakpoint at the beginning of the timer interrupt. 2. Execute the code,…
Other Parts Discussed in Thread: TXS0108E , MSP430F5244 I need to isolate my UART to USB bridge chip (FTID FT232RQ) from my MSP430F5244 so that power does not back feed in my circuit and cause the device to not shut down. I have 65 lines that power could…
Other Parts Discussed in Thread: MSP430F5242 , MSP430F5244 , MSP430F6433 , MSP-TS430RGC64C Hi,
I have problem with programming/reading/verifying/erasing MSP430F5242 with Elprotronic FET-Pro430 (programmer MSP-FET430IUF from Texas Instruments). SW return…
Other Parts Discussed in Thread: MSP430F5244 , SN74LVC1G3157 Hi,
I want to use SN74LVC1G3157 in my application with MSP430F5244 mcu. In test circuit I have made connection between Select signal of
SN74LVC1G3157 to one of gpio of Mcu. When the mcu…
Joe Shidle said: Project Properties -> General. Under the "Device" cluster, there's a drop-down for "Variant". Was set to "MSP430F5229", selected "MSP430F5244". I don't remember if this automatically changed the "Advanced Settings" -> "Linker command…
Thank you
I use the msp430F5244 with 32KHZ XIN and 12MHz XT2IN so start up should be fine with low speed oscillator. After power up i would increase Vout up to 2.2V. However without any pull up or pull down I'm warried about TPS62742 stratup itself…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"