Part Number: MSP430F5338 Hi Experts,
Our customer is currently use one of your microcontrollers in their medical devices (MSP430F5338) - NFBGA package. Due to supply constraints, they have been entertaining alternative chips.
Referring to this post below…
Part Number: MSP430F5338 Hi experts,
Please let me confirm following question,
If 5V is applied externally, is it safe to assume that the voltage is NG since it is VCC+0.3V, but the leakage current of the diode is ±2mA maximum, so the rating of the current…
Part Number: MSP430F5338 Other Parts Discussed in Thread: MSP430WARE , MSPWARE Tool/software: Code Composer Studio Champs,
customer needs to upgrade a project that was originally developed long time ago using CCS4 and msp430ware_0_00_00_10. as a side note…
Part Number: DRV8213EVM Other Parts Discussed in Thread: MSP430F5338 , UNIFLASH , DRV8214EVM , With control GUI 1.1.3, the GUI will connect to the EVM, but as soon as I select Driver Control, it tells me there is new firmware available. When I go and select…
Part Number: MSP430F5338 Tool/software: Code Composer Studio MSP430F5338: I setup the ADC12 with the following code:
//Allow ADC12_A to control Reference (as opposed to control via REF section) REFCTL0 &= ~REFMSTR;
//Turn ON ADC12 ADC12CTL0 |= …
Part Number: MSP430F5338
Hi experts,
Please tell me about the GPIOs of MSP430.
Q1:If P3.0 suddenly changes from high to low, is it possible for P3.1 to be affected by the internal circuitry and thus change the state of the pins?
My customer currently…
Part Number: MSP430F5338 Using the internal reference at 2.5V. When I select
//Set ADC12MEM0 conversion to use internal VREF+ as reference ADC12MCTL0 |= ADC12SREF_1;
there is a region of varying input voltages that cause the output counts to stick at…
Part Number: MSP430F5338 In this case, using STE from Master as a chip select.
Hypothetically, what happens if STE goes active, we receive 1 bit then STE goes inactive. If this happens 8 time (let’s say over hours of time). On the 8 th bit will we…
Part Number: DRV8462 Other Parts Discussed in Thread: , MSP430F5338 Hi! Following my other post ( https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1315642/drv8434s-spi-example-not-working-with-f280025c-launchpad ) - in addition…