Part Number: MSP430F5358 Hi team,
In our design we are using MSP firmware upgradation via I2C using Custom Bootloader. In that flash memory of MSP is divided into Dowload partition, App partition and App manager partition. The binary is sent from Master…
Part Number: MSP430F5358 Hi
In the above snippet, i have selected SELREF for XT1CLK and ACLK,MCLK,SMCLK is driven by XT2CLK. In case if my XT2CLK fails then it will go to DCOCLKDIV which is driven by XT1. And when XT1 fails then it will go to REFCLK…
Part Number: MSP430F5358 Hi, Whether hardware flow control RTS and CTS support available in MSP430F5358 and example code for hardware flow control for this series
Part Number: MSP430F5358 Hi team,
We are using MSP430F5358 IC as the board management controller(BMC) in our project and we have some queries related to this IC.
1. The BMC's oscillator has failed and the BMC's clock is not supplied. In this scenario…
Part Number: MSP430F5358 Other Parts Discussed in Thread: MSP-FET Hello,
We are in the process of a bringing up a new design using the MSP430F5358 using the MSP-FET and CODE Composer.
The Interface to the MSP430F5358 is via a MSP-FET Connection:
The…
Part Number: MSP430F5358 Other Parts Discussed in Thread: MSP-FET Hi
We are using this controller (MSP430F5358) and the MSP-FET Emulation tool.
when we tried to flash through JTAG via CCS, it gave the error of MSP430: Error connecting to the target: The…
Part Number: MSP430F5358 HI Team,
We are using IIC communication between processor and controller. We are having multiple sensor monitoring data and some memory write and read operations on controller, where these operations need to be done by processor…
Part Number: MSP430F5358 I would like to program/debug using FTDI FT4232H in JTAG mode connected to the MSP430F5358 JTAG pins.
How do I add/use FTDI Driver in CSSv10.4 to use the FTDI instead of the MSP430FET ?
Thanks,
Shubhanshu Rastogi
Part Number: MSP430F5358 Hello there ,
I want to flash my MSP through normal UART not from BSL UART, because I am able to perform the communication from it, so wanted to use the same for flashing.
Kindly mention if any possibility and changes I need to make…