Part Number: MSP430F5419A Hello,
I have a product where we need to send a string to a slow serial peripheral (9600 baud) and the messages can be about 100 bytes at a time. I currently have this working tx function:
unsigned int i, len; len = strlen(_ptr…
Part Number: MSP430F5419A Hi Team
Can you help with the inquiry below?
I would like to know whether configuring a pin (port5, pin4) as a peripheral prevents its current value from being updated in the PXIN register.
working with an ADC chip that is connected…
Part Number: MSP430F5419A Hi,
Referring to the screenshot below that I saw in your site, I further need help in deciphering this Lot Code: 16CGS1TG4.
Kindly help advise on the ones with questions:
1 – year - is this 2001 or 2021? 6 - month - J…
Part Number: MSP430F5419A Hi experts,
I have a qeustion about I2C SCL tHigh and tLow.
Formulas for calculating the minimum values of tHigh and tLow can be found in DS.
My customer's I2C has the following settings.
UCBRx:64
fBRCLK:25,000,000(25MHz…
Part Number: MSP430F5419A Other Parts Discussed in Thread: TCA9548A Hi experts,
My customer wants to connect to the TCA9548A over I2C (400kHz).
TCA9548A requires I2C clock low time to be more than 1.3usec.
The MSP430 has an I2C clock low time of 1.25usec…
Part Number: MSP430F5419A Hi,
MSP430 user's guide has the following formula for I2C SCL:
I think this formula has no margin. Is it the correct formula?
For example if I want to use I2C at 400kHz, the minimum values for tLOW and tHIGH are:
UCBRx…
Part Number: MSP430F5419A Other Parts Discussed in Thread: MSP430F5419 , Hi team,
My customer wants to compare the following data between MSP430F5419A and MSP430F5419. -Solderability -Temperature characteristics -Noise immunity -Durability Can I get these information…
Part Number: MSP430F5419A Hi Experts,
Good day.
From SPRABB3 document section 20 VIAS (page 15), it is suggested that a mechanical drill can be used to make a 10 mil via with 5 mil hole. Is this just for a via from outer layer to next layer down, or is…
Part Number: MSP430F5419A Hi champs!
Customer asks, because MSP430F5419AIZCQW is EOL:
Is MSP430F5419AIZCA a drop in replacement (MicroStar => nFBGA package) ??
Part Number: MSP430F5419A Other Parts Discussed in Thread: UNIFLASH [MSP430F5419A BSL] Quesion about jump to RESET VECTOR at BSL routine, FOR EXIT BSL
Hello, Iam naru. I would like to ask help for using BSL, about jump to RESET VETOR at BSL routine.
I…