Part Number: MSP430F5437A Due to component shortage, I would like to temporarily replace the A type by the standard type.
I found a general difference concerning operating voltage range and current consumption of the core.
Who can tell me which other…
Part Number: MSP430F5437
In the MSP430F5437 datasheet, is the ADC "Input Capacitance" the same the sample/hold capacitance and is the "Input MUX ON resistance" the same as the ADC internal series resistance. I'm not familiar with the terms being used…
Part Number: MSP430F5437 Other Parts Discussed in Thread: MSP430F5529 , MSP430F5438A Hello TI Forum,
I've noticed a difference between TA1 and TB0 when running in UP mode, and TOGGLE ouput pin mode.
Both timers use identical configurations (exactly…
Other Parts Discussed in Thread: MSP430F5437 , MSP430F5327 , MSP430FR2355 , MSP430FR5959 , MSP430I2041 Hi Folks,
we've been using the MSP430F5437 for a couple of years in a hand held device that is equipped with an ethanol fuel cell sensor. Years ago we choose…
Part Number: MSP430F5437 Other Parts Discussed in Thread: Z-STACK , CC2538 Are there any known issues relating to OSAL NV element write reliability? I am seeing an issue with data corruption (not just random bit flips) but it looks like the data ended up…
Part Number: MSP-GANG Other Parts Discussed in Thread: MSP430F5437 , , MSP430F5437A Hi,
some trouble prograaming the MSP430F5437 via BSL with the Gang Programmer.
ERROR 68: FBSL initializiation error.
The cable length is 150mm. The connection should be…
Part Number: MSP430F5437A Other Parts Discussed in Thread: MSP430F5437 , Hi,
I have this TI microcontroller with part number "MSP4305437A Rev F" on it.
But when I connect it to the flashpro via JTAG and do an AUTO PROG., I see the following error…
Other Parts Discussed in Thread: MSP-GANG , MSP430F5437 , MSP-FET Hello, I am currently reviewing the MSP430F5437 Device Erratasheet, recently updated in June 2016 to add the Errata "JTAG27". This errata describes an issue where "The device can unintentionally…
Part Number: MSP430F5437A Other Parts Discussed in Thread: MSP430F5437 , MSP430FR6043 , Hi,
Is there a register I can read to know the Die revision number of the microcontroller?
Regards
Lakshmi
Other Parts Discussed in Thread: MSP430F5437 Hi,
I'm using an MSP430f5437 as modbus master and using a MAX3471 as RS485 transceiver.
and this is how I set the uart:
P3SEL = (BIT4+BIT5); // P3.4,5 = USCI_A0 TXD/RXD
UCA0CTL1…