Part Number: MSP430F5438A Hi,
I need the pad placement/package size information as well as any handling/process information available for the MSP430F5438ACY - it should be a die package.
There's another post which says that the package information is…
Part Number: MSP430F5438A Hi
I have a design where I use the MSP430F5438A
I want to upgrade the MSP software via an External uController via I2C
The M430F5438AMGCARET support BSL only on UART pins which are not connected on my design .
Can I upgrade…
Part Number: MSP430F5438A Hello,
I would like to debug the MSP430F5438A and configure the clocks - including timer clocks - to stop when hitting a breakpoint. According to the documentation SLAU208P I can see that the controller has a EEM which is capable…
Part Number: MSP430F5438A Hi,
1.What are the factors for setting the interrupt flag?
2. I'm trying to configure the GPIO interrupt to only happen from high to low [Falling Edge], but the flag is set to 1 at the time the pin goes from low to high. What…
Part Number: MSP430F5438A Other Parts Discussed in Thread: MSP430F2013 Hi Team,
We have planned to use below parts in my design. All below parts are Die package. Kindly please share die package visual images, packing image and assembly details.
Kindly…
Part Number: MSP430F5438A Hi Team,
I am using MSP430F5438AMPZREP on my board. 1. To program the flash memory or RAM using a UART serial interface whether only Transmit, Receive, and GND signal is sufficient. 2. Can we use USB to UART cable TTL-232R-3V3…
Part Number: MSP430F5438A Hello,
I have a customer using the MSP430F5438A in a housekeeping MCU application where they need to keep the power supplies to the system enabled while a firmware update is occurring.
If they have the internal application jump…
Part Number: MSP430F5438A I need to implement a PWM on the MSP430F5438A to support a backlit device. The device is connected to pin 1.1
I found an example that provided a method to setup Timer A0 0 and Timer A0 1 to produce a PWM.
Below is the code:
P1DIR…
Part Number: MSP430F5438A Hello,
we have on our board a msp430f5438a, but for a new feature the ram is not suffisant. so I want to know if you have a µC which should have exactly the same pinout but with more RAM.
best regards,
Part Number: MSP430F5438A We need a simulation model of the MSP430F5438A that will run our code. This is needed for system verification and debug. TI must have one for their chip development. Is there any way to get access to it? Perhaps with an NDA? …