Part Number: MSP430F5438A-EP My customer has the following question:
The transient event below occurs during operation.
The component is an MSP430F5438AMPZREP and the question is whether or not its IO pins could handle a 50mA transient for 20nS when…
Part Number: MSP430F5438A-EP Other Parts Discussed in Thread: MSP-FET Hello.
I am using a MSP430F5438AMPZREP.
I am getting confused about the JTAG connections necessary to program w/ the MSP430FET.
I didn't find a schematic anywhere specifically for this…
Part Number: MSP430F5438A-EP Other Parts Discussed in Thread: UNIFLASH , MSP430F5438A , MSP-FET hello everyone!
I have a few question for BSL and .bin file.
In my situation, i made a custom board using MSP430F5438A-EP. The custom board should upload Fimrware…
Part Number: MSP430F5438A-EP Hello,
I am planning for BSL via UART (not pins).
In SLAU319AF, is this part a "F5xx"?
In SLAU319AF, Table 1-1, is this part described by the column F5xx non-USB?
If not, is there anything except the SLAS967A datasheet…
Part Number: MSP430F5438A-EP Other Parts Discussed in Thread: MSP430F5438A Hi Experts,
Our customer would like to know if there is an associated dev kit with MSP430F5438AMPZREP?
I do not see any devkit for the mentioned device. However, I check a catalog…
Part Number: MSP430F5438A-EP Other Parts Discussed in Thread: MSP-FET , TUSB3410 , MSP430F5438A Hi,
I'm trying to get the MSP-EXP430F5438 (Rev 03) board working as described in the documentation (slau263i). Hardware/connections are:
IC = MSP430F5438A…
Part Number: MSP430F5438A-EP
Hello! everyone.
I want to trigger the ADC12 with Timer B.
My plan is Timer B triggers ADC12 about once per 0.1 second.
I configurated the timer B and ADC12. But it didnt worked. where am i missing?
I understood if i SHS…
Part Number: MSP430F5438A-EP Using the MSP430F5438A-EP microcontroller component whose temperature range is between -55 and 125 degrees Celsius In our project there is an external OSC XO 25.0000MHZ LVCMOS component that connects to the input of pin 89…
Part Number: MSP430F5438A-EP Hello. TI Team.
I have a problem. How to select BSL Pin?
These pictures were taken from MSP430F5438A-EP datasheet.
This is BSL Pin requirements and functions.
Ths is Terminal Function and Port P1 Pin Function.
The Second…