Part Number: MSP430F5508 Other Parts Discussed in Thread: MSP-FET Hi good afternoon,
I'm trying to program the MSP430F5508 using the Programmer MSP-FET Flash Emulation Tool and the Software SmartRF Flash Programmer, but an error message is gotten from…
Part Number: MSP430F5508 Team,
As MSP430F5508IZQER (JRBGA) is flagged as obsolete, customer will like to know if we have any PCN or relative document, and if there's any drop-in or similar alternative within/out MSP430F5508 portfolio that they can refer…
Part Number: MSP430F5508 Other Parts Discussed in Thread: UNIFLASH , Hi,
I tried to download the example code included with SLAA514.
In this example, the device is set to F5510.
I have several F5508.
So I changed the device setting to F5508 and got the …
Part Number: MSP430F5508 Hello, I need to connect an IMU sensor, an SD card and a GPS to the MSP430F5508. I couldn't find the SCK and SS pins for the SD card. This is my first problem. My other problem is related to communication. SPI pins are also i2c…
Part Number: MSP430F5508 Hello team,
Our customer is looking for the device which is supporting “USB to UARTs (two CDC functions)”. Currently, customer is interested in MSP430F5508 and they are asking if TI has sample-code which has “USB to…
Part Number: MSP430F5508 Other Parts Discussed in Thread: MSP430WARE Tool/software: Code Composer Studio Hi
In a USB keyboard application developed with CCS using MSP430F5508, the number of key code transmission data may be changed from 8 bytes to 9 bytes…
Part Number: MSP430F5508 I cannot seem to program the MSP430F5508 using BSL-scripter when connecting it to an older PC with Sandy Bridge chipset. It works to flash the RAM BSL but after that it does not accept the program file. When trying the same on…
Part Number: MSP430F5508 Dear support,
I have a device with the below command to enter to BSL. The below command worked with over 1K of devices in the field, but in the new batch assembled the MCU instead of entering BSL reset itself immediately,
USB_disconnect…
Part Number: MSP430F5308 Other Parts Discussed in Thread: MSP430F5508 Tool/software: Code Composer Studio Hi,
We designed a board based on MSP430f5508 micro controller. we use USB in our design to talk to the Host PC. USB device is not detected by the…
Part Number: MSP430F5508 Other Parts Discussed in Thread: MSPBSL
Hi
I wish to BSP program my device via USB. I am using the python usb firmware upgrader, powering up while pressing the RST but the device is not recognized. what am I missing?