Part Number: MSP430F6459 Other Parts Discussed in Thread: MSP430F5438A , MSP430F5438A-EP , MSP430F6458 Hi,
The TI MCU selection tool allows one to select MCUs based on RAM / IO, or other peripheral counts. However, I know that not all MCUs that are suggested…
Other Parts Discussed in Thread: MSP430F6659 , MSPWARE , MSP430F5358 , MSP430F5359 , MSP430F5658 , MSP430F5659 , MSP430F6458 , MSP430F6459 , MSP430F6658 Hi,
anybody used successfully the MID (memory integrity device) on an MSP430F6659 Rev A?
On my MSP430 dumping…
Other Parts Discussed in Thread: MSP430F6458 Hi,
I'm working on an application using a msp430f6458 and I'd like to add a LCD.
Power consumption is very important to me, and I need to display 4 characters (4*8-segments). Those characters need to be…
Other Parts Discussed in Thread: MSP430F6458 , MSP430F6736 distribution FAE said:
Is it possible to generate 20 MHz MCLK in MSP430F6458 using 32768 kHz watch crystal on XT1 LF mode? Any challenges?
You would not use XT1 directly, but you can use XT1 as…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…