Part Number: MSP430F6730
Hi Team,
Our customer would like to know what is the ENOB of our MSP430F673x and MSP430F672x controllers.
Thank you for your support!
Regards,
Danilo
Part Number: MSP430F6730 When the chip is in power down,According to the design of the peripheral circuit, it needs to be configured to output high-level mode or input mode after power-off. However, it is found that after being configured as input, the…
Part Number: MSP430F6730 Now a certain product of our company (using MSP430f673 series chips), found the following picture to describe the problem; At present, 32.678khz crystal oscillator is adopted in the hardware, and the main frequency of configuration…
Part Number: MSP430F6730 I have some confusion regarding 24 bit sigma delta converter
1. I am not able to find the exact time duration between from tigger of conversion till the 24 bit sample results are obtained. THe OSR 1024 and modulator sampling…
Part Number: MSP430F6725A Other Parts Discussed in Thread: MSP430F6723 , MSP430F6723A , , UNIFLASH , MSP430F6730 , MSP-FET Tool/software: Code Composer Studio When installing the MK (MSP430F6725A IPN (TI) on the device card in replaceable MSP430F6723A IPN…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…