Part Number: MSP430F67651A Other Parts Discussed in Thread: MSP430F6435 Hi, I'm using MSP430F67651A for my project, but the crystal oscillator (XT1)isn't working.
I had a similar problem with MSP430F6435, but now it works with the code for Unlock…
Part Number: MSP430F67651A Hi, I got a question from my customer using MSP430F67651A. He wonders whether it is possible to input high frequency clock (~24MHz) to XT1. Register configuration : UCSCTL1:0021h(DISMOD=1b(Modulation disabled)) UCSCTL4:0000h(SELA…
Part Number: MSP430F67651A Other Parts Discussed in Thread: MSP430F67651 , Tool/software: Code Composer Studio Hi, My customer has been using MSP430F67651 with compiler version 5.51.1. Now they are considering to use MSP430F67651A. Does the same compiler…
Part Number: MSP430F67651A Hi Team, I would like to ask for assistance with our customer inquiry below for MSP430F67651A:
1. What is the value of the internal reference voltage of the 24-bit and 10-bit ADCs of MSP430F67651A when gain = 1?
2. What is the…
Regarding ...
Carl Hagenmaier said: SDSCM00046695 SDSCM00046115
These appear to be very small floating point computation errors very similar to CODEGEN-4323.
Thanks and regards,
-George
Part Number: ADS1298 Hello,
I have done all the initialization of ads1298 and i can read registers wit POL=1,PHA=0,
when i read channel data which is C00000,8*(800000)
I do not get anything with this setting.
I am receiving wrong register data with…
Sir my controller is msp430f67641a
My problem is that in msp430f67651a port 1.4 & port 1.5 is work as a uart/spi communication so how can I am migrate this pin work as a i2c communication.
Other Parts Discussed in Thread: MSP-GANG , MSP430F67651A , MSP430F67651 Hello Team,
One of my customers is using MSP-Gang for programming MSP430F67651A. They use two MCU in this system and during production they first program other MCU. This MCU might do…