Praveen,
I'm not sure I understand your issue. The MSP430F67661A has 6 USCI modules, all of which can provide a SPI interface. The dedicated Chip Selects (CS) for the device is a particular form of SPI that is to normally used. The general solution for…
Hi, Praveen
Praveen N1 said: Is it possible to do it in TIDA-00454 firmware?
It's possible.
Praveen N1 said: Then what kind of modification, do I want to carry down on the circuit?
Circuit measures Ua,Ub,Uc with one common point AGND.
What you need is…
Part Number: MSP430F67661A Dear Team,
I have been engaged in measuring AC three-phase using MSP430.
Could you please provide information on the minimum and maximum differential voltage that can be read via SDXP0 and SDXN0?
I need to measure…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Other Parts Discussed in Thread: CC2640 , CCSTUDIO , CC2538 CCS not detecting installed compiler tools in Windows Docker container for CI build Hello all BACKGROUND: I'm trying to set up a CI build for a CC2640 processor using a Windows Docker container. I…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave