Part Number: MSP430FR2311
Hi,
just to make sure that I have understood correctly, is it so that MSP430FR2311 does not support JTAG fuse blowing function?
And so I do not need to care about Fuse Blow Protection Resistor either in SBW-interface?
Thank…
Part Number: MSP430FR2311 I want to use UART BSL to write a program to MSP430FR2311 but I couldn't.
I caught a picture of signals "RST#", "TEST", "UCA0RXD", "UCA0TXD"
After entry the BSL mode, first, TXD's voltage…
Part Number: MSP430FR2311 Hello,
I have a customer trying to use SLAA760 as a reference for their Linux implementation of an MSP430 BSL programmer. I just wanted to point out that the BSL protocol here only works for the 2/4 series MSP430's and not the…
Part Number: MSP430FR2311 I am trying to use the external reference output of 1.2V on the MSP430FR2311. Even though I enable the external reference, when I run the program, the EXTREFEN remains at 0 and the reference output on P1.7 remains at 0V.
#include…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP430G2553
Hi,
When creating a default empty project in CCR 12.4 for a MSP430FR2311, the --code_model compiler flag is set to large. This has a significant effect on the program memory footprint…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: MSP430WARE
Hi,
I'm running into a problem with a MSP430FR2311. Please see the code below. When I remove the RTC ISR pragma, the TimerB ISR is never called (!).
#include <msp430.h>
#define…
Part Number: MSP430FR2311
Hi,
I am trying to make a variable persistent using the PERSISTENT pragma. The code is a copy of an example made by Andreas Dannenberg (posted somewhere on the TI forums):
//=================================================…
Part Number: MSP430FR2311 Hi all,
I suspect that I am having an issue with LPM 4.5. I am programming a game and after flashing the MSP 430, nothing happens - none of the LEDs light up. When I have the device connected physically and I manually go down…