Part Number: MSP430FR2522 I am developing a keypad (cap-touch), using MSP430FR2522, now i want to integrate with a host controller (preferably with MSPM0 controller). I developed a custom PCB using MSP430FR2522 and able to detect the touch (key press…
Part Number: MSP430FR2522 Other Parts Discussed in Thread: MSP430FR2422
I am trying to read ambient temperature with an MSP430FR2522 using the internal temperature sensor.
I am using the calibration data ( link ) stored in the device to convert the ADC…
Part Number: MSP430FR2522 Hi,
use MSP430FR2522.
Due to firmware burning error, the IC cannot be recognized when burning again? Is there a solution?
thanks!
Part Number: MSP430FR2522 Other Parts Discussed in Thread: MATHLIB I am getting the compiling error:
>> Compilation failure captivate/ADVANCED/subdir_rules.mk:9: recipe for target 'captivate/ADVANCED/CAPT_Manager.obj' failed "../captivate…
Part Number: MSP430FR2522 Other Parts Discussed in Thread: MSP430FR2422 , , MSP-GANG , MSP-FET , UNIFLASH Hi,
We are using 2 MSP430 mixed in 1 product, a MSP430FR2522 and a MSP430FR2422 which is fine for us and helps with availability.
At the moment we are…
Part Number: MSP430FR2522
Hi team,
Could you share the max / min number for VLO at LPM 3, 4 ? Datasheet says the typical number is 15% but there is no description for max / min number in the datasheet.
Table 5-8 in the datasheet mentioned there is two…
Part Number: MSP430FR2522 Hi, I am noticing large temperature drift when the circuit is heated, the temperature of the sensed object doesn't noticeably affect the raw count. For example;
Count dry
output
Count wet
output
y=mx+b
Temp
x1
y1
…
Part Number: MSP430FR2522 Other Parts Discussed in Thread: MSP-TS430RHL20 , I have an MSP430FR2522 plugged into the socket of the MSP-TS430RHL20 eval board. I have modified the loopback example project and have the UART working on P1.4 and P1.5. I have…
Part Number: MSP430FR2522 Other Parts Discussed in Thread: MSP430FR2422 , , MSP-FET Hi,
I got some boards from our production line that did not pass our board tester, they failed on the MSP bootloader program step.
We are using MSPFlasher 1.3.16 with the…