Part Number: MSP430FR2675
Hi everyone,
I would like to know if it's possible to dynamicaly set the capacitive touch parameters of my MSP430, ie conversion count, proximity and touch thresholds. I tried to set parameters as noinit so I can change the…
Part Number: MSP430FR2675 Hello,
I am writing a couple of drivers for various sensors that the MSP430 is communicating with as an I2C master. I have the code below that I have been using to write/read data via the I2C. It has been working well.
I2CMaster_error_t…
Part Number: MSP430FR2675 I am working on updating the MSP430FR2675 FW via I2C using the msp430-i2cbsl-tool tool. I am sending this command "./msp430-i2cbsl-tool -i /dev/i2c-0 -s a -f Cerberus.txt" and I get the following error.
------------…
Part Number: MSP430FR2675 I have an MSP430FR2675 that is communicating with an Ambarella CV25 MPU via I2C. The CV25 is the master and the MSP430 is the slave. I have set up my MSP430 to be able to handle I2C slave communication with a master. I have tested…
Part Number: MSP430FR2675 Hello,
I am new to TI products and had a question that I could not resolve in the datasheet or application notes.
On the MSP430FR2675 there is a pin called VREG. The datasheet gives a values for a capacitor to place next to this…
Part Number: MSP430FR2675 Hi,
I am working on fixing an issue that we are seeing in manufacturing and believe I have found a bug in the driver library for the MSP430FE2xx_4xx parts; version: 2.91.13.01.
We are seeing an issue when we set the clock up…
Part Number: MSP430FR2675 Other Parts Discussed in Thread: UNIFLASH Hello,
I am using CCS version 12.0.0.00009 to program an MSP430FR2675. I have been able to run debug programs on the MSP430 for the last few days without any issues. However, today, I…
Part Number: MSP430FR2675 The issue occurs on a product with more than 500k unit produced (without significant MSP430 issue).
We got report from production that some part (we are fetching exact figures for now) have low power issue (wirth no software…
Part Number: MSP430FR2675
Hi,
Good Day.
Customer is trying to modify the msp430fr267x_euscia0_uart_01.c code example to run on EUSCI1 at 115200 baud. Can you confirm that these settings are correct?
UCA1BR0 = 4; // 8000000/16/115200 UCA1BR1…