Part Number: MSP430FR5969-SP Other Parts Discussed in Thread: MSP430FR5969 Hi,
I was wondering if you have any IBIS simulation models for the MSP430FR5969 device.
Thanks!
Part Number: MSP430FR5969-SP Hi experts
Can someone provide more details regarding the applied pin and supply voltages, ambient and/or junction temperature and configuration of the device for the respective radiation test reports?
There isn't much detail…
Part Number: MSP430FR5969-SP Hi,
I noticed in the datasheet, it mentions that SPY Bi-Wire can be used to interface with MSP430 development tools and device programmers.
Does this prevent me from using this on my board without these devices? In other…
Part Number: MSP430FR5969-SP Hi,
I would like to have the option of programming the MSP430 by either the JTAG (4 wire) interface or by using a microprocessor to program it over the BSL interface. I have a drawing of it below and was wondering if this…
Part Number: MSP430FR5969-SP Hi,
I am trying to test out the following code on the eval board with little success: msp430FR59xx_eusci_uart_standard_transceiver
I now have two eval board where one is sending TX data at 115200 to the other but the other…
Part Number: MSP430FR5969-SP Hi,
I wanted to interface to the MSP430 device. I noticed in the MSP430 datasheet, it lists the digital I/O specs like positive going input threshold voltage etc.
I was wondering if I use these specs for the following interfaces…
Part Number: MSP430FR5969-SP Other Parts Discussed in Thread: MSP-FET Hi,
I have the MSP‑EXP430FR5969 evaluation board along with a version of CCS. I am able to run a few of the SW examples provided. The eval board is connected via the USB interface to…
Part Number: MSP430FR5969-SP The UART transmitter cannot be selectively depowered and is normally high. It’s voltage is leaking through the deenergized MSP430 and is pulling up the 3.3V power rail up to about 1.9V. The MSP430 datasheet only specifies…
Part Number: MSP430FR5969-SP Hello,
I'm looking to use the MSP430FR5969-SP for a space flight product which requires radiation hardened components. The MSP430FR5969-SP has the HFXT input for a tuning fork crystal, but there does not appear to be radiation…
Part Number: MSP430FR5969-SP We're using an MSP430FR5969-SP microcontroller for our application, and we noticed that the temperature coefficient of the internal MODOSC clock source seems to be higher than called out in the datasheet.
Without getting…