Part Number: MSP430FR6047 Hello, I have a problem about Uart communication with MSP430FR6047. I'm using Serial interface SN65HVD1781D of TI, see Datasheet below. I connected my TD on P2.0, RD on, P2.1, DE on P1.6 and RE on P1.7 my First question is…
Part Number: MSP430FR6047
hello I would like to inquire about the calibration of msp430fr6047. We are attempting to calibrate from Q1 (0.00625m3/h) to Q4 (3.125m3/h). First, as a result of checking the meter constant measured in Q3 (2.5m3/h), the meter…
Hi Aravind,
Please see our published example codes and modify them to change the port and i2c device address. You can find all of our examples at the SDK path I mentioned in my previous responses. You can also find examples by exploring our TI Resource…
Part Number: MSP430FR6047 Other Parts Discussed in Thread: TIDA-01486 Hi,
We were developing a solution with MSP430FR6047 flow meter. The flowmeter board actually works well and we are getting valid flow rates from flow meter module. After taking reference…
Part Number: MSP430FR6047 In an example of assembly on "Ultrasonic Leak Detection" I was able to obtain information on the use of "Jiakang 1 and 2 MHz" transducers. Could you recommend other brands of these frequencies? I would need to be able to get…
Part Number: MSP430FR6047 Hi, I'm trying to flash an MSP430FR6047 with a Raspberry Pi 4, does anyone have done it before? now I'm using Debian GNU/Linux 12 (bookworm) as OS on the raspberry and a J-TAG to flash the MSP430 with my windows PC, and other…
Hi Umut,
thanks for the update. You can confirm this is closed by clicking the resolved button. Thanks. I saw your latest entry and will let our experts follow up on this.
Regards, Frank
Part Number: MSP430FR6047 Hello,
I have a problem with the MTIF module. I have conducted some tests with it and I noticed that the interval between pulse transmissions is not constant.
The module's frequency is set to 128Hz (PGFS_3), and the frame duration…
What areas are “Device descriptor info(TLV)(FRAM)” and “TI calibration and configuration(FRAM)”? Is the area used dynamically when the EVM430-FR6047 operates? Or, I wonder if this is an area where users can read and write to arbitrary…
You should be able to use an external voltage divider and the internal 1.2 reference from REF_A.
If you want your maximum voltage to be 4 V (to give yourself some headroom), you would set the divider for a 0.3 ratio.