Part Number: MSP430G2131 Other Parts Discussed in Thread: DRV8838 , DRV8838EVM ,
Hi,
We are using MSP430G2131 on DRV8838EVM. We are using the provided DRV8838_CustomerEVM_Default_Code.c
DRV8838_CustomerEVM_Default_Code.c
//******************…
Part Number: MSP430G2131 Other Parts Discussed in Thread: DRV8838EVM , DRV8838 , MSPWARE , MSP430WARE We are planning on using MSP430G2131 on DRV8838EVM. The datasheet for DRV8838 MCU mentions that to expand beyond the included firmware capability the MSP430…
Part Number: MSP430G2131 Other Parts Discussed in Thread: DRV8838 Hi,
We are trying to establish SPI between MSP430G2131(slave) and CH341A(master) to control the potentiometer. The goal is to read the potentiometer data from the DRV8838 EVM board and transfer…
Hi Dennis,
We are planning to use one of the ADC channels. I read on the datasheet that the ADC module contains built-in voltage reference with 2 selectable voltage levels.
Is there any particular advantage of using internal reference compared to external…
Hi
Apologies. We are still using one timer to generate 2 PWMs. Assuming one of the PWM has frequency = 20 Hz and Duty Cycle = 20%. That means that the period is 50ms (with high time = 10ms. i.e. CCR0 register goes up to 1000 counts).
We want to wait for…
Part Number: MSP430G2131 Other Parts Discussed in Thread: MSP-FET , DRV8837EVM , DRV8837 Tool/software: Code Composer Studio sir usb fet was not connected error comming while debugging. i am checked with the device manager compared with msp4302553 in this…
Part Number: MSP430G2131 Other Parts Discussed in Thread: MSP-FET , MSP430G2744 , Dears:
We use FET430UIF emulator to download code with SBW interface, and we find the time is about 2 minutes.
Is it normal to use 2 minutes? Since the code is not big.
Pls…
Part Number: MSP430FR2111 Other Parts Discussed in Thread: MSP430G2131 , Tool/software: Code Composer Studio Hey everyone!
Hello,
I am working with a motor driver evaluation module ( DRV8837EVM ) where I have replaced the existing MCU (G2131) with an FR2111…
Part Number: MSP430FR2111 Other Parts Discussed in Thread: DRV8837EVM , Tool/software: Code Composer Studio Hello,
I am working with a motor driver evaluation module (DRV8837EVM) where I am replacing the existing MCU (G2131) with an FR2111.
The idea is…
Part Number: MSP430G2131 Other Parts Discussed in Thread: TIDM-MSP-DALI , MSP430G2452 Hi team,
a customer is looking for complete Dali master-slave solution.
We have the SLAA422 solution with MSP430G2xx. The questions are:
- As it is not explicitly described…