Other Parts Discussed in Thread: MSP430G2202 , MSP-FET Hi,
I have developed a device that uses the MSP430G2202 using the Launchpad. The chip works inside the final product well.
I have a programming rig setup (A shield with a ZIF socket on the launchpad…
Part Number: DRV8711 Other Parts Discussed in Thread: MSP430G2202 , TIDA-00736 , , MSP430G2553 Hi TI Experts
I am looking for the sample code for MSP430G2202 on TIDA-00736. Would you please provide it ?
Note: Just for your information, this design has the…
Dear Duncan;
Thanks for reply.
TIDA-00736 is include MSP430G2202 , and this design allow step and current setting by switch.
I think, MSP430G2202 may inclde different code.
Regards
Once again, the MSP430G2202 is supported by the MSP-EXP430G2 eZ430 so I am just as perplexed by the issue. At this point I can only recommend sky-wiring the FET to a G2201 device (with RST & VCC components) to see if there is an issue with the board…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited by…