Part Number: MSP430G2402 Other Parts Discussed in Thread: MSP430FR2111 Hi
Looking for low cost MCU with below requirements:
Minimum of 12 GPIO
0.5KB RAM
8KB/4KB ROM/FLASH
Minimum 256B Internal runtime reprogrammable FLASH
Minimum 1x16bits timer (from…
Part Number: MSP430G2402 Hello,
The MSP430G2xx supports External Digital Clock Source. When an external clock is input to XIN (P2.6), can P2.7 (XOUT) be used as GPIO?
Also, when I checked the data sheet, I found in the explanation of P 2.7 that the Pin…
Part Number: MSP430G2402 Goog Morning TI community!
Today I have a question about programming FLASH memory's MSP430 processors.
I use some segments of the Info Memory as EEPROM to store data, so I write on it several times during the execution of…
Hi Lukas!
I see about 15 fails at the moment and every board has uP with this word: MSP430G2402, 34KG4, CF30A.
I really need to find what is the exact problem in order to resolve it as soon as possible, so, if you have any ideas please let's discuss it…
Part Number: MSP430G2553 Other Parts Discussed in Thread: MSP430FR2475 , , MSP430G2402 TI Friends and Family,
Our customer has found a peculiar anomaly between ID Codes on FR2475 and targeted G2553. Comments welcomed!
[Customer}
I am getting our manufacturing…
Part Number: MSP430G2402 Goodmorning TI Community,
Today I write to You because of a strange problem with some elecrtonic board on which there is the MPS430G2402 processor.
After some work cycles the processor stops working well and gets lost.
The origin…
Interrupts with improper interrupt handling can cause this.
You don't have any global variables, so after a reset, the code almost instantly starts. Then you may enable some interrupts and the CPU jumps into the void, resetting or crashing. At this time…
Part Number: MSP-GANG Other Parts Discussed in Thread: MSP430G2402 , , MSP430G2232 During this seemingly unending semiconductor shortage, I needed to change the microcontroller on an existing PCBA to one that was actually available to purchase. Ended up…
Other Parts Discussed in Thread: MSP430F5438A , MSP430G2402 Hi All,
Will greatly appreciate if someone can provide some references where I can find source code to read the Microchip 24AA02 EEPROM. I need code that works with the USI on the MSP430G2402.…