Part Number: MSP430I2021 Hi Team,
Do you see any way of keeping the voltage on MCU Rx below the max of Vcc+0.3V (Vcc=3.3V) in the schematic below? The boards have already been manufactured and resistors can't be altered anymore.
Thank you,
Fra…
Hi Benjamin,
I'm not sure I follow your question here. VFSR and absolute voltage are different specifications. VSFR defines the max voltage the ADC can resolve. Absolute voltage max defines the max voltage the device can take before you risk damage.…
Other Parts Discussed in Thread: MSP430I2021 , MSP430G2553 Hello guys,
I have a project based on MSP430I2021 and it has no external clock source, crystal or oscilator, so I need to use DCO.
I am using CCS v7.
Also I want to use Timer module to occur 1ms…
Hi William,
Thanks for posting your question on E2E. For future posts, please use a more descriptive title, not just the part number. One of the purposes of the forum is to allow other community members to search for similar questions and answers. If…
Hi Dennis,
The engineer used MSP430I2021 without CVREF, and asked me is it ok? what would happen with no CVREF, a larger or smaller CVREF?
I think CVREF can reduce noise of Vref and help to get better performance. And I suggested the engineer add a CVREF…
Part Number: MSP430I2021 Hi,
Can anyone help me to find the DC offset value in the DC removal filter applied for the single-current meter?
Regards,
Minal Barad.
Part Number: MSP430I2021 Hi,
while giving heat to the device controller stops working, only core voltage is okay otherwise all peripherals stop working.
after reset in runtime also it's not okay, I have to on/off the whole device to make the controller…
Part Number: MSP430I2021 Hi experts,
Let me check the setting of the EUSCI register (UCBRSx) in the following system.
SMCLK = 16.384MHz/4 = 4.096MHz N=4.096MHz/38400bps = 106.6666...
In the above case, which is correct?
Rounding up the decimal point: …
Part Number: MSP430I2021 Other Parts Discussed in Thread: MSP-EXP430F5529LP Hello,
I'm trying to connect the MSP-EXP430F5529LP.
After programming MSP-EXP430F5529LP with the firmware TI_MSP_HIDBRIDGE__1_00_04_00__MSP-EXP430F5529LP.txt
I get No connected…