Part Number: MSP432E401Y Dear,
On our custom board, build around the MSP432E, we use the CRC module. Before using the CC module, we reset and enabl the module as on Ti reconditions.
Once in in a while, after cold booting the board, the READY bit does…
Part Number: MSP432E401Y Other Parts Discussed in Thread: CCSTUDIO Hi,
I Installed Code Composer Studio in windows11, Version 12.6. But It shows some error.
java.lang.ExceptionInInitializerError at com.ti.chromium.browser.ChromiumBrowserContributor.createBrowser…
Part Number: MSP432E401Y Hello
I am able to generate the CRC of individual flash sections during link time using the following in the cmd file
.text : palign(4) > FLASH, crc_table(crc_table_for_text,algorithm= CRC32_PRIME) .const : palign(4) > FLASH…
Part Number: MSP432E401Y Other Parts Discussed in Thread: UNIFLASH , Hello
I was using Uniflash Version 7.0.0.3615 to program the MSP432E401Y on a target CCA. I believe I have locked the device via the "Settings & Utilities" "Lock Device" option. I was…
Part Number: MSP432E401Y Other Parts Discussed in Thread: UNIFLASH , Hello TI E2E community,
I’ve been utilizing the UniFlash tool on Windows to flash code and program MAC addresses onto MSP432E401Y devices. Recently, I discovered a helpful tip in the…
Part Number: MSP432E401Y Hello. I have the following question for MSP432E401Y: How do I study the corresponding register pin by utilizing the data sheet?? Who is the responsible pin for PWM in MSP432E401Y?? And how will I know that??
Part Number: MSP432E401Y Other Parts Discussed in Thread: UNIFLASH Hello
I am having trouble with programming two applications to flash.
One application is only a constant structure which contains configuration data that will be used by the executable…
Part Number: MSP432E401Y Hello Everyone,
i am making msp to go to lpm0....in lpm0 I am getting 2.2mA...please let me know what is reason for this issue. how much will comp_e, Timer A and ADC14 module will consume current....?
is there any idea to check…
Part Number: MSP432E401Y Hello
I am working on a Nuclear Safety related embedded application using the TI MSP432.
I am trying to make use of the capability to create, using the linker a CRC for a zone of data in FLASH and to then be able to, during startup…
Part Number: MSP432E401Y In MSP432E401Y datasheet, the Maximum current per output pin is mentioned as 64mA.
As per the below statement in the datasheet, GPIOs are configurable only upto 12mA
How much is the maximum current per output pin?
Is it possible…