Part Number: MSP432P411V Hello. I have the same problem and Chris answer is great but ¿How can I tell sysconfig I'm using 401V variant instead of 401R? My project properties has 401V variant and consulting the sysconfig configuration at the project's…
Part Number: MSP432P401V Hi, My customer is looking for MCU which is capable Live Firmware update in field. In customer’s scenario, MCU needs to be working continuously while new firmware is loaded from an external host via UART, i.e. there are…
Part Number: MSP432P401V Hi Team '432,
I have a customer question..
The Datasheet says “The main memory can be viewed as two independent identical banks of up to 1MB each, allowing simultaneous read or execute from one bank while the other bank is…
Part Number: MSP432P401V I am converting existing and generally-working UART RX code at 115200 to DMA because an occasional character is dropped. I disabled the currently-used EUSCI_A_UART_RECEIVE_INTERRUPT and wrote the following code to implement DMA…
Part Number: MSP432P401V Hi Team SimpleLink,
Any Advice / Docs / AppNotes etc WRT Porting Software / Code from TM4C123BH6Z to MSP432P401V?
Thanks, Merril
Part Number: MSP432P401V Hi Team 432,
Some questions WRT P401 & P4111..WRT TI Drivers.. Driver_Lib.. Flash APIs.. SDK format/structure.. 432 sampe code/projects..
1. Seems the 432 SDK has changed a bit in content & structure..
a. The 432 SDK used…
Part Number: MSP432P401V Tool/software: TI C/C++ Compiler Hi,
1.We are going to use our (MSP432P401VIRGCT) for our product. We need the clarity of information memory and flash memory write operation. If we flash our code to flash memory, going to era…
Part Number: MSP432P401V Tool/software: Code Composer Studio Good evening,
I am currently trying to reproduce the datasheet specifications for above MCUs. While successful with the 401R variant, I did not suceed with the 401V one.
I am using the MSP-EXP432P401R…
Part Number: MSP432P401V Hi,
What's the max baud rate of eUSCI as UART?
And what's the TX and RX error at that baud rate?
Customer's request is 5Mbps.
Thanks a lot.
Br, Jordan
Hi Amber,
My mistake. Try referring to this example: http://dev.ti.com/tirex/explore/node?node=AOdkyKTrMt781Uyuxf0WVw__z-lQYNj__LATEST
The MSP432P4111 uses the same FlashCtl_A as the MSP432P401v
Thanks,
Alexis