Part Number: MSP432P401V Hi,
I'm following Kobi's suggestion in previous thread . Now, I Have a query regarding this. Do, I need oad_bootloader.c kind of file to have a update for msp432 with CC3200.
Although I'll be using custom bootloader to…
Part Number: MSP432P401V I created code to sample multiple channels continuously. I triggered it with MAP_ADC14_toggleConversionTrigger(). This code was based on an example in the C:\ti\simplelink_msp432p4_sdk_3_20_00_06\examples\nortos\MSP_EXP432P401R…
Part Number: MSP432P401V Hello,
While trying to compile the driverLib `spi.c` against the MSP432P401V part using IAR I receive the following errors:
Error[Pe020]: identifier "EUSCI_B1_BASE" is undefined ....\spi.c 467
Error[Pe020]: identifier…
Part Number: MSP432P401V
Hi All,
I have downloaded the firmware file via UART as Kobi suggested in previous post . My query is how I can update the firmware image of MSP432 with that file.
Thanks,
Keshav Aggarwal
Part Number: MSP432P401V Hello,
I am working on a custom board which has the msp432p401V on board.To understand things better,I started my development with the msp432p401R launchpad and created an example which works fine at 48MHz clock.I changed my example…
Part Number: MSP432P401V Hi All,
I'm working on a project where I have 2 individual devices MSP432P4 and CC32xx(CC3200/ CC3220) running different host applications. I'm able to OTA update the firmware of CC32xx.
Is it possible to use CC32xx to…
Part Number: MSP432P401V Apparent Bug with ti\simplelink_msp432p4_sdk_3_20_00_06\source\ti\devices\msp432p4xx\driverlib\cs.c. When I include cs.c in my project to access a function that is not in the ROM Library, cs.c includes debug.h, which refers to…