Other Parts Discussed in Thread: ONET8501T
Hola TI,
Can someone help provide me the parameter of ONET8501T as below:
PARAMETERS
MIN
TYP
MAX
UNIT
TIA RSSI
Slope
?
?
?
mA/mA
…
Other Parts Discussed in Thread: ONET8501T Hi,
My customer is using ONET8501T. He would like to know recommend information for wire bonding. Detail of information is "Caution at wire bonding", "recommend wire diameter" and "tool for bonding". Could…
Other Parts Discussed in Thread: ONET8501T , ONET8541T , ONET8531T , ONET8551T Hi
My customer is working on ONET8501T. He is connecting a two terminal PD. Can i get some advise on which is the best way to connect up?
Ivan
Other Parts Discussed in Thread: ONET8501T Dear Team:
We know ONET8501T unstressed sensitivity typical is -14dBm.
Could tell me the value range (min.~max.)?
Thank you
Part Number: ONET8551T Other Parts Discussed in Thread: ONET8521T , ONET8501T , ONET8541T , ONET8531T Hello,
I was performing a review on your ONET- series of transimpedance amplifiers for a new product we are working on. These include:
ONET8551T…
Hi,
I think you should be able to use the ONET2591TA with an APD reverse biased at 140V and without using the filter pin. As a result, there will be no DC current reading on the RSSI pin.
A higher speed version than the ONET2591TA would be the ONET8501T…
Other Parts Discussed in Thread: ONET8501T , ONET8551T We are currently developing a 10Gbps module and are considering the TI ONET8551T for the transimpedance amplifier stage of the design. With the expected variances in the photodiode/current source…