Part Number: OPA129 Hello, I would like to know the meaning of the marking , at the third and last line of OPA129UB part: I think it's Trace code , but h ow to find date code from this trace code ? Thanks... (98A03N)
First Line = B BB OPA
2nd Line…
Hi Team, Our customer is using the old OPA129 in their existing design. They are looking to migrate on active products but would like to clarify some things for comparison purposes. The OPA129 datasheet uses the asterisk (*) symbol in its typical characteristics…
Part Number: OPA129 Hi all
We are using a OPA129UE4 which now is obsolete. Is there a pin-compatible replacement type with similar spec? The OP is used as photodiode amplifier.
Thank you
Best regards
Part Number: OPA129 Hi,guys!
I have a plan to make Voltage Follower.
Apply Input voltage about 0 ~6 V
I have two questions.
First, There was no information about Common-Mode Input range condition.
I'd like to know the specific conditions.
Second…
Part Number: OPA129 Hi,
I've seen the OPA129UB is mark end of life.
It is a critical part for us and I would like to know if there is a direct replacement?
Thanks
Dany
dgagne@ldetek.com
Part Number: OPA129
We are interested capturing EEG signals ( using ADS1299 ). Its said in the datasheet the input impedance is around 1Gohms. For our specific task we need to have more higher input impedance. Could we achieve it by adding a high impedance…
Part Number: OPA129 Hello,
I've noticed that the OPA129 and OPA128 performance as spec'd on their datasheets is very similar. Is the different package (SOIC vs TO99) the primary difference between the parts, or is the design of the die also different…
Part Number: OPA129 Hi,
I am using OPA129 as an non inverting amplifier for an in put range -0.5V to +0.5V , but whenever I dont give an input to the non inverting pin( leaving it floating), It picks up a very small noise( its freq is ~50 Hz ..guessing…
Part Number: OPA129 I am considering integrating a photodiode with a trans-impedance amplifier and was wondering if the OPA129 is available in die form?