Hello,
I figured out what was wrong with this ESD issue. I had too strong and un-calibrated ESD source. I pushed complete design above the ESD limits. After several testings with calibrated Teseq NSG435 ESD gun, the product has 8kV-contact/15kV-air…
Part Number: OPA1678 Thanks .We have used the opa1678 for Automobile audio, we want the POWER and the output ues one line,as follow:The automobile give us 8V (DC),then it get sounds(AC) from the 1678.
We wang Frequency Response as the attachment …
Part Number: OPA170-Q1 Other Parts Discussed in Thread: OPA1678 , OPA170 , OPA2172-Q1 , OPA2172 Hi Sir,
The OPA1678.tsc works normally for 25KHz BPF, but the replacement of the OPA170 works abnormal. What is wrong? OPA1678.TSC OPA710.TSC
Part Number: PCM5102A Other Parts Discussed in Thread: OPA1678 , LM27762
Hi,
Sometime ago I asked you a question about possibility of using op-amp with PCM5102A to have higher Vrms at lower loads than 10k and you recommended me to use something like…
Hi na na78,
I'd suggest the following circuit:
This will give you 55dB out to a 32kHz (52dB, or -3dB point). In order to use the OPA1678 as a noninverting buffer in this case, you'll need to bias the input to mid-supply. However, if only the noninverting…
Part Number: OPA1678 We have used OPA 1678 For microphone ,we want to the Frequency Response as attachment {Frequency Response of OPA 1678 }.But the actual Frequency Response as attchment {The actual Frequency Response }. Our schematic diagram as attachment…
Part Number: TLV9144 Other Parts Discussed in Thread: OPA1678 Tool/software: Hi team,
We were interested in this device because of its low power consumption, and when we replaced it with a device from another company, it picked up a lot of external…
Part Number: NE5532 Other Parts Discussed in Thread: OPA1678 Tool/software: Hello TI team, I am reaching out because I’m currently assisting a customer, Ember Industries, Inc. They have contacted us regarding some issues they are experiencing with the…
Hi Li Ning,
Ning Li said: pls kindly help to check if there have changes to the internal structure?
You are likely dealing with the new FAB NE5532 product, see the PCN link below.
https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/5726…
Part Number: OPA1688 Other Parts Discussed in Thread: OPA1678 , OPA1637 , , OPA344 Tool/software: Hi Team,
Customer is trying to design the OPAMPs circuit for MEMS MIC output, and they are looking for a lot of OPAMPs for this design. So please review…