Part Number: OPA2134
I obtained some OPA2134PA DIP op-amps from a friend to test. For my test circuit I am using:
+/- 13.5 volt supply, 100 nF and other bypass caps
Signal input 4.5 Vpp sinewave, 65 KHz, centered at 0V
Gain about 4 (RG/RF)
I have parts…
Part Number: OPA2134 Hi Experts ,
Referring to the TI SIEP notification SOIC package need to be returned due to some process changes .
We have a stock of MPN : OPA2314UA/2K5 of DC 2240. Refer to below label where we need to understand whether these…
Part Number: OPA2134 Other Parts Discussed in Thread: OPA1656 Hi team,
Is it possible to drop-in replace OPA2134UA/2K5 with OPA1656IDR?
Best regards, Antoine
Part Number: OPA2134 Hello TI Support Team,
Mouser Electronics received a request from a customer with two parts. As noted on attached images, one part received has one notch and the other has two notches.
Can you explain why one notch is present and the…
Part Number: OPA2134 Anyone had experience on this part marking? what's the " 1" "2" or "A" on the first line stand for?
Does the "A" is for suffix UA for the part number?
thank you!
Part Number: OPA2134 Other Parts Discussed in Thread: OPA1656 , OPA134 Hi Team,
My customer wants to replace OPA1656 with OPA2134. Which one has better electrical characteristics? will replacement of the chip affect the sound?Any things should take into…
Part Number: OPA2134 Other Parts Discussed in Thread: OPA2314 Hi experts,
These were from Arrow.
During our inspection, we decapped a piece of OPA2134AIDGKR with DC:1915. The die did not show any markings that relates to a OPA2134 series.
Please check…
"In order to input 2Vrms, I think that Gain should be under 1 because Vcc is 5V."
This part won't work (well) with a single 5V supply. Choose an op-amp that will, such as OPA2365.
Part Number: OPA1656 Other Parts Discussed in Thread: OPA2134 , OPA2604
The OPA1656 is the industry’s lowest voltage noise high voltage CMOS on the market. It offers exceptional performance in almost any audio application. The low voltage noise combined…
Part Number: OPA2134 Other Parts Discussed in Thread: TINA-TI , OPA134 , Tool/software: TINA-TI or Spice Models I'm not sure if there is a lib or olb for the OPA2134 as I can't find one. From the datasheet and spicerack it only links it to the OPA134. I…