Part Number: OPA2197 Other Parts Discussed in Thread: MSP430F6726A , TINA-TI , OPA197 Hi
The OPA2197 is operated with both ± 6V power supplies.
At this time, the -6V power supply contains ripple noise of about 10KHz,
so I inserted a 680Ω and 1μF…
Hi TonyMCC,
The OPA2197 is a very high performance operational amplifier used in many applications such as industrial control, automation, medical, etc. It's characterization information seen in the datasheet is centered more so on those types of applications…
Part Number: OPA2197 Other Parts Discussed in Thread: OPA2197 , OPA2188 HI, I am using opa2197.
When the following circuit is operated, the output switches.
AO_O wave.
Adding a bypass cap 10nF to ao_0 will not cause this switching. The problem…
Part Number: OPA2197-Q1 Other Parts Discussed in Thread: OPA197 Hi team,
My customer wants to verify what is the output voltage swing and input common mode range for OPA2197-Q1 across the full temperature range(-40 ~ 125deg)?
Thank you.
Best…
Part Number: OPA2197 Other Parts Discussed in Thread: TINA-TI , OPA197 I am having some trouble with the SPICE model in LT SPICE.
It runs extremely slow in LT.
I did notice that the model for the 2197 is a lot more complex than the other installed…
Part Number: OPA2197 Other Parts Discussed in Thread: TINA-TI , , OPA2192 Tool/software: TINA-TI or Spice Models From the data sheet I understand both OPA2197 and OPA2192 are very similar, other than offset related specifications.
I have imported OPA2192…
Part Number: OPA2197 Other Parts Discussed in Thread: OPA197 , LF353 I'm using the OPA2197 dual opamp in an inverting opamp summing junction with 3 input signals. The device is powered from +/-12Vdc. Each input signal consists of an 25Khz to 60Khz 2Vpp…
Part Number: OPA2197 Other Parts Discussed in Thread: TLV6700 Dear Team,
If my customer wants to monitor Vout voltage, do you have suitable reference design and use which part number?
They want to monitor Vout rail, if Vout is higher or lower the…
Part Number: OPA2197 Hello team,
How can I think about offset voltage drift in near V+ rail condition?
Datasheet shows offset voltage drift specification with Vcm=(V+)-1.5V as test condition. At same time, OPA2197 Vcm range reaches to V+ rail.
Does…