Part Number: OPA2209 Other Parts Discussed in Thread: OPA827
1. In the below chart Input current Noise Density versus Freq., Wondering to know if most OPAs has such behavior or 500 fA/Hz value?
2. When OPA2209 is place in front of the ADC as a buffer…
Part Number: OPA2209 Other Parts Discussed in Thread: OPA209 , TS321 , OPA2197 , TINA-TI Hi Support team
My customer adopted OPA2209 as the current sense, hope the delay can be as small as possible. Please help to see if there is any value that can be a…
Part Number: OPA2209 Other Parts Discussed in Thread: OPA209 , , TINA-TI I was using Tina TI to build a filter circuit using the OPA2209. I used the macro in the Tina library and my circuit was working fine. I was on line and I noticed a new PSpice file…
Part Number: AFE58JD28 Other Parts Discussed in Thread: OPA2209 I tried to configure the circuit to have a range of -0.4 V to +0.4 V in CVNTLP, VCNTLM. However, the circuit is not working.. U18's OUTPUT does not change even though the DAC OUTPUT value…
Part Number: ADS8688
Dear team,
I am testing our ADS8688A EVM and my input signal is a DC voltage from 0V to 5V.
Use the input range of 0~5.12V,
connect the OPA2209 filter between input DC signal and ADC input pin. then the ADC output error is extremely…
Part Number: OPA2209 Other Parts Discussed in Thread: OPA209 , Hi All,
for the opamp OPA2209AIDR can you please let me know at what forward voltage does the back to back diodes on the opamp input terminals start conducting 10mA of current?
Part Number: OPA2209 Hi
OPA2209AIDGKR is used.
customer's circuit is as below, which is used to sample LLC output 12V power rail current.
the power for OPA2209 is 12V comes from auxiliary power.
when AC power is plug in, auxiliary power flyback works…
Other Parts Discussed in Thread: OPA2209 Hi,
I simulated the following amplifier circuit using OPA2209. Input is 2.5VDC. Output has ripple voltage instead of 5VDC output.
Can you please tell me what could be the cause for this behavior? I attach the Ltspice…