Part Number: OPA244 This Analog Application Journal states that WEBENCH Amplifier Designer could be a useful tool for photodiode amplifier design.
Where's this tool? I'm not able to find it in TI site.
Part Number: OPA244 Other Parts Discussed in Thread: TLV1805 , LM5112 Hi,
I need to drive a few FET to about +-15V (digital) while using a minimum of quiescent current and boaed space (0.5mm or larger pitch is preferred, though).
Speed is not critical …
That recommendation is wrong; the TLV9101 is not a slow, low-power opamp.
The speed scales with power. Low-power alternatives would be the TLV2401/TLV6003 (5.5 kHz, 0.9 µA), OPA251 (35 kHz, 27 µA), or OPA244 (430 kHz, 50 µA). There is no reason to replace…
Part Number: OPA244 Other Parts Discussed in Thread: TLV2451 , , OPA348-Q1 , TLV2381 , OPA347 , OPA348 Hi all Would you mind if we ask some opamps? About below amps, which amps are JFET or bipolar type? We are sorry that we could not judge correctly. As our recognition…
Part Number: OPA244 Hello, can anyone please confirm for the short circuit curve given in the datasheet does +Isc stand for current sinking and -Isc for current sourcing ?
Other Parts Discussed in Thread: OPA244 Hi
Is "ESD Capability 2,000V "of OPA244 "HBM" or" CDM "? (which of MBM or the CDM is it?)
(Data sheet page5)
Best regards
Other Parts Discussed in Thread: OPA379 , OPA244 Hello, all
Now we are considering to use OPA244 or OPA379 for our next model.
I am referring each datasheet, but I could not find out find out the output current information when applying Vcc=3.3V.
We need…
Part Number: LM309 Other Parts Discussed in Thread: LM358B , OPA244 , TLV9302 , LM358 QUAL AMPLIFICADOR OPERACIONAL MAIS MODERNO PODE SUBSTITUR,
DE FORMA ADEQUADA, O AMPLIFICADOR OPERACIONAL OBSOLETO LM308
DO CIRCUITO ABAIXO?
Other Parts Discussed in Thread: OPA244 , XTR111 , OPA237 , TINA-TI Dear Sir ,
I use one OPA244 for generated a 4-20mA output but with this OPA a don't have a stability in temperature
Have you a solution or another OPA???
Thanks
Your faithfully
…
Hi Elisha,
Please check out OPA244 and LMC6041. Both these devices are available in single channel 8-Pin SO package. I've included few specs below, but I would highly recommend going over the datasheets.
Best Regards,
Bala Ravi