Part Number: OPA2835 Other Parts Discussed in Thread: TINA-TI I trying to simulate a circuit that amplifies a differential input, that comes from a inductor with two coils, and the comom wire is connected to reference voltage of 0.8VDC.
The circuit is…
Art Kay said: I think a better option is to use a simple op amp buffer.
Hello Art Kay ,
I came across your reference design "Low-Side Current Shunt Op-Amp Circuit to Single-Ended ADC for Cost-Optimized Monitor"
I have a query, assume in the above…
Part Number: OPA2835 Hello, 1. In the OPN, OPA2835IDGS, DGS stands for the package, right?
2. Does "I" have any meaning? It seems that all part numbers listed in the datasheet all have "I" Thank you!
Part Number: OPA2835 Other Parts Discussed in Thread: OPA2837 , OPA2836 , OPA838 , OPA2834 Hello,
I would like you to confirm how TI measure "crosstalk vs frequency" figure of OPA2835.
Could you please send us measurement environment(including…
Part Number: OPA2835 Let me start of by saying Thank you TI,
Got caught with wrong info on the above chip. We downloaded the RUN package .bxl and pin 4 and pin 5 are swapped in the schematic symbol.
Made 8 boards costing us nearly USD5000 just in manufacturing…
Part Number: OPA2835 Hi
I downloaded the .bxl for the RUN package of the above chip from the TI website. The schematic library symbol has pin 4 and 5 swapped.
Pin 4 is labeled VS- and Pin5 is labeled PD1. The data sheet shows the correct pin out and it…
Part Number: OPA2835 Quick question: is the only difference between the OPA2835IRMC and OPA2835IRUN the height of the package? They appear to have an identical footprint and pinout.
If I don't have height constraints, is there a particular reason to select…
Hello John,
The designer was able to run some extensive simulations on the input impedance of the OPA835 and here are the numbers that came out:
Common-Mode Impedance (on each pin): 100MOhm || 2.2pF
Differential Impedance: 400kOhm || 0.1pF
I will…