Part Number: OPA2990 Our customer asked about the weight of the OPA2990IDSGR I have to see the PACKAGE OUTLINE in the data sheet did not include the weight and silicon-based transducer
Part Number: OPA2990 Other Parts Discussed in Thread: OPA990 , Hi,
I would like to know if OPA2990IDR (Dual, SOI-8) and OPA990IDBVR (Single, SOT 23) include shutdown feature.
According to pins assignments in both devices, there is no SHD pins. Does it mean…
Part Number: OPA2990 I am curious about ESD. Are the CMOS op amps more susceptible than the older Bipolar op amps? For example the OP275G (actually that one has a JFET front end).
Part Number: OPA2990 Hello TI
I would like to use an OPA2990SIDGSR (or maybe different housing type) in a circuit and therefor I would like to know, if it is possible to apply voltages of up to 30V to the OpAmps output pin, when the output ist shut down…
Part Number: OPA2990
Hi Team
My customer is try to make a S/H circuit using the OPA2990, and they want to know whether the open-loop or the close-loop is better for this application considering the accuracy.
Also, is the follower output or the integrator…
Part Number: OPA2990 Hello. I have a question about the absolute maximum rating of the supply voltage of the OPA2990IPWR. It is stated that the minimum supply voltage is 0 [V] in the data sheet. However, when I measured the voltage before the power was turned…
Part Number: OPA2990
Folks,
I'm writing to confirm the SHDN functionality and thresholds. I believe that the SHDN function works like so:
SHDN
Logic LOW = (V-) to (V-) + 0.2V = Amplifier enabled
Logic HIGH = (V-) + 1.1V to (V-) + 20V= Amplifier…
Part Number: OPA2990 Hi support team.
My customer would like to know when is RTM for DGK package(VDSSOP-8).
Please let me know if you could provide the information about it.
Best regards,
Higa