Part Number: OPA316-Q1 Other Parts Discussed in Thread: OPA316 The OPA316 PSpice model cannot work with CST(A EMC relevant simulation tool), the reported error is as below, could you please help? My customer said there is no such issue with other suppliers…
Part Number: OPA316 Other Parts Discussed in Thread: TIPD204 ,
Hi,
While referring to this design (TIPD204, refer fig.1 pasted below), I was not able to understand, why 49.9 Ohm ( R TERM) resistor is being used in parallel with the input signal. Is it to…
Part Number: OPA313 Other Parts Discussed in Thread: OPA316 , OPA314 , , TINA-TI Current issue is that I am comparing some circuits using OPA313, OPA314, and OPA316 pspice models. If I simulate identical circuits using OPA313 and OPA314 in the same schematic…
Part Number: OPA316 Hi team,
Could you please share the FMEDA file of TPS7B6950QDCYRQ1 so that my customer can use it to do system level analysis? You can reply to me through emails. Thanks.
Part Number: OPA360 Other Parts Discussed in Thread: OPA361 , , OPA316 , OPA858DSGEVM , THS7372 , THS7368 , THS7364 , THS7360
Dear Team,
we have some design questions regarding OPA360/OPA361
1) If the OPA needs to be enable all the time is it better to leave…
Part Number: OPA316 Other Parts Discussed in Thread: OPA837 , LMH6601 , OPA838 , , TLV9062 , TLV9002 Dear Sirs, could you clarify the correctness of the different configurations for the SC-70 and SOT23 please.
Datasheet SBOS703F –APRIL 2014–REVISED OCTOBER…
Part Number: OPA316 Other Parts Discussed in Thread: TINA-TI Hi!
I have recently designed a simple non inverting amplifier using the OPA316. Here are the key parameters:
+IN: Connected to GND
-IN: Input signal (-200mV to 0V)
Supply: V+: +3V, V-: GND
…
Other Parts Discussed in Thread: OPA316 , OPA827 [ OPA316 ] General Questions, Gain, Gain Error/Flatness
Hi, Sorry that it's not specific question related to OPA316. However, if I draw the relationship between input and output voltage as below, * Gain…
Other Parts Discussed in Thread: OPA316 , TIPD154 , OPA317 1. I have application where input signal voltage varies from +5V to -5V. Have to level shift the signal and fed it to microcontroller adc which is sampling at 1MSPS. Microcontroller adc range varies…