Part Number: OPA4187 Other Parts Discussed in Thread: OPA192 Dear TI experts,
My customer wants to make bandpass filter as the specification below ;
frequency : between 0.3Hz and 2.5Hz
Input signal : 20mV sine wave
Designated output signal : 2V
Amplification…
Part Number: OPA4187 Other Parts Discussed in Thread: LM4040 , MUX36D08 , , ADS8318 , REF5020 , OPA4192 Unexplained noise showing up in multichannel temp data acquisition system. Advice sought.
Background:
All bridge, ADC reference voltages generated from…
Part Number: OPA4188 Other Parts Discussed in Thread: OPA4187 We are trying to do AC and Transient modeling of a circuit with the OPA4188 and OPA4187 with TINA, and would like to get spice models for these devices. Where do we go to look for device models…
Part Number: OPA4187 Hi,
The chopping frequency is 125 kHz, but is it OK to use as 3rd order LPF of 3 kHz? And do I need to add a filter that suppresses 125 kHz?
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/947368/opa187-chopping…
Part Number: OPA4187 Can you please provide the thickness of each substance found in the NiPdAu terminal finish of part OPA4187IPW ?
Is the thickness composition for this part the same for all TI parts that come in TSSOP-14 package?
Is it the same for…
Not higher slew rate, but higher bandwidth. Just compare the OPA4187 and the OPA320.
The supply current (also called "quiescent current") of OPA4187 is only 100µA. The supply current of OPA320 is 1.45mA. So choose an OPAmp consuming about 1...2mA.…
Part Number: OPA4187 Other Parts Discussed in Thread: OPA187 , , OPA387 I have a question about the closed loop gain of OPA4187IPWR. Please refer the attached file.
6082.OPA4187IPWR.pdf
Part Number: OPA4187 Other Parts Discussed in Thread: OPA187 Hi Team,
If the (noninverting) input (pin 2) gets a voltage in the range of +/- 2,4 .. 3,5 V I see a corresponding output as expected only in the negative range. The positive voltage is limited…