Part Number: OPA4196 Other Parts Discussed in Thread: OPA196 Dear Michael, good day!
Thank you
Excuse me, I have not clearly understand about additional resistor 10 k.
You wrote: "2. Can it be set to a zero output current mode - no, it can't - at minimum…
Part Number: OPA4196 Other Parts Discussed in Thread: TINA-TI , OPA2990 , TLE2071 , TLE2141
Dear Michael, dear Thomas, thank you.
Please, answer
I will use amplifier for the next purpose: I need to generate positive and negative pulses 5...14 V amplitude…
Part Number: OPA4196 Other Parts Discussed in Thread: BUF634A Dear Thomas, please answer
I decided to use booster with OPA4196. I need to increase output current. Please, see my circuit in attach.
VG1 - is the DAC with output voltage from 0 to 3 V, then…
Part Number: OPA207 Other Parts Discussed in Thread: OPA2202 , OPA2196 , OPA4196 , OPA4197 , OPA2197 , OPA4202 I am looking for a 2 and 4 channel equivalent of the OPA207.
Please make any recommendation that will satisfy this need.
Part Number: OPA4196
Hi. I have question about OPA4196's package.
According to device information in datasheet, OPA4196 has TSSOP package.
But TSSOP Package is not existed in packaging information.
OPA4196 has TSSOP pacakge or not?
Part Number: OPA4196 Hi,
Do you have a plan to release Q1 device for either following devices?
1.OPA4196IDR
2.OPA4197IDR
3.OPA4192ID
4.OPA4277MDTEP
Best Regards,
Hide
Hi Adam
What package of the LMC6482 (dual) and LMC6484 (quad) is the customer using today? Spec-wise the OPA2196 (dual) and OPA4196 (quad) are great upgrades!
See the package options below and spec comparison here: https://www.ti.com/compare-products/…
I did try using r value of 365 Ohm and 9.09K Ohm but still saw the same issue as I had with the higher value resistors. I then tried the OPA4196 both with my lower value resistors and the original value resistors and this did resolve the issue I was seeing…
Hi Nuno,
I have found these here:
https://www.ti.com/assets/js/compareParts/compare.html?familyId=1293&parts=OPA4196,OPA4191,OPA4171-Q1,OPA4171,TLV4171,OPA4130,TLV9154-Q1,OPA4991-Q1,TLV9154,OPA4991,TLV9354-Q1,TLV9354,TLV2444,TLV2444A,LMP7704&cols=o1,p3318…
Hi Xu,
By all accounts the OPA4188 is an electrically superior replacement for the legacy LM224 ( I think you meant LM224, LM244 is a non-TI LED). However, because they are so different in design and electrical performances from each other that could…