Part Number: OPA4322 Other Parts Discussed in Thread: TINA-TI
Hi OPAMP folks,
I'm doing TINA simulation with OPA4322 as an unity gain buffer. Could you help advise for its operation?
What I'm trying to do :
I want to implement an unity gain…
Part Number: OPA4322 Hi there,
I'm considering OPA4322 to boost the current drive capability as DAC I'm using can drive only +/- 15mA and I require more than 25mA. It seems that OPA4322 can typically drive +/-65mA, is it correct? If so, can you…
Part Number: OPA4322 Other Parts Discussed in Thread: TINA-TI , OPA4376 Hi,
Our customer is considering adder circuit with OPA4322 and simulated with TINA-TI but saturation was seen saturation as following.
Their requirement is
- Add offset 1.65V for…
Hi Brian,
Your timing is really great for this. We just released the OPA4323IPWR and I would recommend choosing that over the OPA4322.
Both devices (OPA4323 and TLV9064) have different input capacitances. Though both are pretty close to one another.
OPA4323…
Part Number: OPA4322-Q1 Other Parts Discussed in Thread: OPA2348-Q1 , Hello TI Team,
I am using both of the above op amps (OPA4322-Q1 and OPA2348-Q1). When these op-amps are off ( It is possible that (+) input voltage can go up to 16V through a 49.9k resistor…
Other Parts Discussed in Thread: OPA4322 Hi guys,
I've simulated with OPA4322 negative feedback amplifier.
Simulation is observed clamping at 100 mV, while in reality measurement such clamping does not occur.(minimum is GND)
does anybody occur this…
Other Parts Discussed in Thread: OPA4322 Hi Dears,
Could you help to recommend one amplifier which is pin to pin with OPA4322AIPWR TSSOP package,
1) with similar performance, the bandwidth>5MHz is OK; 2) fit for Vcc=2.7-5.5V application; 3) The Vol at…
Hi Sean,
there's almost never a 100% replacement. But the OPA4322 looks like a good candidate.
Keep in mind, that the TSV994 seems to be a decompensated OPAmp and needs a minimum gain of 4.
Kai
Part Number: TDC1000 Other Parts Discussed in Thread: LMV881 , OPA353 , OPA357 , , OPA322 , OPA4322 , REF2912 Hello. I am testing the Ackerberg-Mossberg bandpass filter and have questions. The filter enters the generation mode and it worries me a lot. Generation…