Part Number: OPA838 Other Parts Discussed in Thread: OPA836 , EVM430-FR6043 , TIDM-02003 , Hello Expert,
We changed from OPA836 to OPA838 according on EVM430-FR6043 to what is specified in the TIDM-02003 reference design.
When we changed OPA838 from OPA836…
Part Number: OPA836 Other Parts Discussed in Thread: OPA838 , , OPA837 Hi team,
My customer is using our OPA836 & OPA838 now.
And they wonder if we have a newer device to recommend.
Requirements:
BW: >200MHz
slew rate:>200V/us
Iq:<1mA
Thanks…
Oh and incidentally, way back at the top I had said I thought this was updated - so
2005 I did the original one that you have attached
2010 Karki updated mine using the same quadratic but shifting the target DAC output swings down
Later, I thought the…
Part Number: OPA836 I want to use OPA836IRUNT as a non-inverting amplifier with a gain of +1. I shorted Output (pin1) and inverting input (pin 2). What I should do with pin 6,7,8,9? Can I leave open these pins?
Part Number: OPA836 Other Parts Discussed in Thread: TINA-TI Hi Team,
i was reading our datasheet today but have some confusion with datasheet.
1. when used split power supply with both postive and negative power supply, how to push the OPA836 to power…
Part Number: OPA836 Other Parts Discussed in Thread: OPA837 , OPA2834 , OPA197 Hi team,
My customer is evaluating OPA836 in a water meter project. This project cares about the power consumption very much. Customer found OPA836's Ib is as below:
This…
Part Number: OPA836 Other Parts Discussed in Thread: OPA659 Hello,
How to do a buffer with OPA836?
I attached my simulation, please take a look.
OPA836.TSC
The op-amp operates in single supply of 5V.
The input signal is DC to 60MHz, and the amplitude…
Part Number: OPA836 Other Parts Discussed in Thread: OPA830 , , OPA3832 Hi Team,
my customer is looking for VGA signal driver solution which meet VESA1.1 SPEC,
they are reference MAX4380 & ISL55033 now and asking if we have the similar device which can fit…
Part Number: OPA836 Hello,
Is there a matching spec for the integrated resistors? I understand that they are laser trimmed to +/- 1% accuracy, but want to confirm is the ratiometric matching is better than 1%.
Don