Part Number: OPA836 Other Parts Discussed in Thread: OPA830 , , OPA3832 Hi Team,
my customer is looking for VGA signal driver solution which meet VESA1.1 SPEC,
they are reference MAX4380 & ISL55033 now and asking if we have the similar device which…
Part Number: OPA836 Hello team,
Hope you are doing well. Customer is inquiring about any potential issues with cleaning PCB mounted ICs in ultrasonic cleaner?
Specifically the following op- amps: OPA836IRUN OPA838SIDCK OPA695IDBV
Regards,
Ran…
Part Number: OPA835
Hello,
I am founding lot of problems calculating the phase margin of a circuit.
To measure the phase margin I am using this other circuit, dividing fb(s)/inm(s) at the output.
This is what the output look like, with…
Part Number: OPA836 Other Parts Discussed in Thread: OPA838 , , OPA847 Hello,
I would like to know the possible gain range for OPA836 & OPA838 amplifiers?
Regards,
Jadhav
Hi Shrikant,
What supply voltage are you operating the OPA836 at? As shown in Figure 7, if you are operating the device at +2.7V supply then you will clip at the output for 2Vpp input due to gain of 2. The OPA836 now has to output 4Vpp which is beyond…
Part Number: OPA836 Hello team,
Hope you are well.
Customer is inquiring about any baking instructions for OPA836IRUN.
There were parts which were left in open stock and would like to have them properly dried.
Regards,
Randhir
Other Parts Discussed in Thread: OPA333 , OPA836 , OPA376 Hi
Our project is Grid Monitor Device. We are arranging use TI OPA376 and OPA836 in our project. As our project is very care the EMI performance. So I want to ask if TI can share the EMIRR test…
Part Number: OPA836 Other Parts Discussed in Thread: TLV2362 , Hi team Could you let me know how much high/low subthreshold on PD pin when it is used +/2.5V? Best Regards, Takanori Yuzawa
Other Parts Discussed in Thread: OPA835 Hi ,
which is the value of internal gain setting resistors: 1.6K, 1.2K,400 ohms as at page 4 or 2.4K, 1.8K, 600 Ohms as at page 5? Thanks
Umberto