Part Number: OPT3001-Q1 Please give me the shipping inspection standard of OPT3001-Q1.
The data sheet of this component indicates potential risk of the discoloration, scratches, fingerprint and dust.
I want to understand what kind of shipping inspection…
Part Number: OPT3001-Q1 Dear team,
My customer GWM-NOBO is using OPT3001-Q1 as light sensing. They need the sensing area's position in the IC to decide the mechanical parameter of opening.
Could you please share it?
Part Number: OPT3001-Q1 Hi team,
My customer have questions about OPT3001-Q1 output variation.
・ The following variation in measurement output is approximately +/- 10%. Is the variation from the initial tolerance?
・ In addition, what is the measurement…
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT3006 , OPT3001 Hi team,
As shown in the picture, because it is relatively close to the edge of the revision, I would like to know how small the diameter of the ALS hole on the cover plate should…
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT4001-Q1 Hi Team,
I would like to check if our OPT3001-Q1 and OPT4001-Q1 can meet the spec or not. smoke print spec 14%+-4% in 550nm
Regards,
Roy
Part Number: OPT4001 Other Parts Discussed in Thread: OPT3001-Q1 , , OPT3001
Hello Team, Our customer want to know about following points between OPT4001-Q1 and OPT3001-Q1.
Package and pin assignment compatibility
Operating temp and voltage condition…
Part Number: OPT3001-Q1 We are using custom board with jetson nano, we need to configure interrupt functionality in opt3301 in latched window style comparison mode, as per data sheet we need to clear a bit every time when interrupt occurs. Can you specify…
Part Number: OPT3001-Q1 Hi team,
Is there any risk to block the I2C if reading the result before a conversion is complete?
Customer set the conversion time to 100ms, and the system will poll the result register(0x0) every 100ms. Any risk?
B&R
Liji…
Part Number: OPT3001-Q1 Hi Expert
because of customer PCB board area limit, customer want to use resistor divide circuit for power to OPT3001-Q1.
so my question is:
Does this device supply requirement high or low? can it accept power supply fluctuate…