Part Number: PCA9306 Other Parts Discussed in Thread: TCA4307 , TCA9800 , TCA9509 Hi
The attachment is ltc4307cms8#pbf with PCA9036 to achieve 3.3V to 1.2V, 1 drive 4 function.
There are 2 ltc4307cms8#pbf+PCA9036, each drive 2 FPGas (it is required that…
Part Number: PCA9306 Other Parts Discussed in Thread: TCA9803 , Hi Team,
What is the farthest transmission distance of this device? Customer would like to design an external 1m transmission distance, will the signal attenuate? And how to evaluate it?
The…
Part Number: PCA9306 Other Parts Discussed in Thread: LSF0101 Hello
I am using the PCA9306 to translate from 3.3V I2C to 5V I2C bus. With Vref 1 = 3.3V and Vref2 and EN connects to 5V via 200k res. Is this correct? Is there a capability to simulate the…
Part Number: PCA9306 Hi,
Confused with the PCA9306DQER layout/Footprint of this part.
Didn't understand this note. How to implement this if the selected package do not have a thermal pad.
Part Number: PCA9306 Hi all, my customer noticed a slightly different die size among two same components with similar date code and country of origin. It appears that the DC 2227 (right side in the picture) has a smaller/shrink die size.
Thus, the question…
Part Number: PCA9306 Dear Team,
Can the left and right Vref be connected to 1.8V as a switch? I'm worried that there will be a problem with the internal MOS bias voltage. Thanks a lot.
Many Thanks,
Jimmy