Part Number: PCA9555 Other Parts Discussed in Thread: PCF8575 , Currently I am using PCF8575 IC of IO expander. With this IC , I am facing issue of all pins are high at power on or reset condition. But I require all pins are low at power on or reset condition…
Part Number: PCF8575 Other Parts Discussed in Thread: TCA9535 , PCA9535 VCC 3.3V 입력, 포트는 출력 모드로 사용 중이다. 출력 라인에 기본 풀다운 저항(10Kohm)이 있는 경우 높은 출력 레벨은 3.3V가 아닌 약 2V 레벨로 출력됩니다. 무엇이 문제일까요?
Hi Aleksandr,
As Clemens mentioned, 100mA is a typo. This pull-up current should be 100uA.
Aleksandr Sorokin said: As I understand this correctly the writing pulse (one clock pulse) affects the output.
The state of the outputs change on a successful ACK…
Part Number: PCF8575
For PCF8575, how to estimate the power consumption of the pins, which are used as output GPIO?
Is Ioh the parameter to use?
In the data sheet, Ioh appears in several places with different value:
6.1: -4mA +-100mA (so big?)
6.3:…
Part Number: PCF8575 Dears,
Thanks for your support in advance.
1. Below is the Block Diagram of PCF8575 from datasheet( I marked 1,2,3 three MOSFETS,), in my understanding this P-port is push-pull output (MOSFET2 and MOSFET3),
my question is: when configure…
Hi Bobby Thank you for the reply. Yes. I found the root cause of the problem. We have connected a pull-up resistor on the line between the TPS26625 and the PCF8575. This pull-up resistor is falsly connected to 3.3V and this caused the wrong voltage level…
Part Number: TPS2662 Other Parts Discussed in Thread: PCF8575 Hello
I have a custom board on which the FLT pin of the TPS26625 is directly connected to an IO-Expander PCF8575 input. There is no additional resistor in line or a pull-up or pull-down resistor…
Part Number: PCF8575 Hi,
HTOL is not mentioned in the reliability test results. I have no doubt that the test result is "PASS", but I need to answer the customer.
Could you please provide the following information? "Min lot qty" "SS / lot" "Condition…
Part Number: PCF8575 In our products we use PCF8575PW, but due to unavailability am not able to find the part.
What is difference between PCF8575.PCF8575C,PCF8575D ?
Can you suggest PCF8575 replacement ?
Part Number: PCF8575 I am trying to determine the markings on a pair of PCF8575 IC's to confirm if they are functionally equivalent. Both are TSSOP-24 packages.
One IC is marked
PF575
13G4
A8GH
The other is marked
PF575
OBG4
A3KQ
I understand the…