Part Number: PCM1808 Hi Team,
May I have the PCM1808 sample code or library file for customer?
With this, they can speed up the development time for output signal analysis with their MCU.
Thanks.
Part Number: PCM1808 Hi Team,
I have a question regarding the Analog Input Voltage. When our DUT (Device Under Test) is in idle mode, an input signal activity on VinL and VinR can be generated. During this activity, the signal can go as low as -628…
Part Number: PCM1808 Hello Support Team,
The recommended value for power line capacitors is 100nF with one 10uF electrolytic capacitor as per the datasheet but in EVM all capacitors are ceramic. In the current design, we used all Ceramic capacitors as…
Part Number: PCM1808 Other Parts Discussed in Thread: PCM1754 I'm designing an ADC/DAC with PCM1808 and PCM1754.
My main processor, running linux, has a single I2S bus with 2 data lines (in/out), a bit clock and a select line. Could the 2 devices…
Part Number: PCM1808 Hello,
I'm developing a circuit based on PCM1808. It is basically a PCB with an analog MIC, a preamplifier and the PCM1808 to encode analog signal to digital I2S interface.
I started recording a 880 Hz sine audio source, but the…
Part Number: PCM1808 Hi team,
If PCM1808 is used for frequency generation from MCLK to BCLK + LRCK when there are no AD conversion, is it no problem that Vcc is no supply or 3.3V supplied?
Regards,
Hayashi
Part Number: PCM1808-Q1 Hello,
it is posted here: https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1076843/pcm1808-q1-center-voltage-input-range
"DC blocking capacitor in series with the input - In this case the device self biases the inputs…
Part Number: PCM1808-Q1 Other Parts Discussed in Thread: PCM1808 Hi team,
Are the Mclk and BCLK of the PCM1808 output from the same clock source?
Best Regards,
Haury