Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM1865-Q1 Hello,
I need to use the PM6360 with 64kHz and 128kHz. Unfortunately the chip senses "invalid sample rate" in the ASI_STS register and mutes SDOUT.
I managed to bypass the PLL and…
Part Number: PUREPATHCONSOLE
Tool/software:
A table with links to all the software needed for audio devices and their EVMs. Find the device(s) of interest in the table and use the links to request access to the software you need.
Product or…
The PCM1840 is a 113dB/123dB 4-channel, hardware-controlled audio ADC and this device is suitable replacement of AK5384.
For more flexible software-controlled quad-channel ADCs, TLV320ADC3140 (106dB), TLV320ADC5140 (108dB/20dB) and TLV320ADC6140 …
Dear Diego-san
Thank you for your information.
Please allow me to have one more question.
We see SNR ofr SE is -106dB for PCM1865-Q1.
Test Conditions:
0-dB PGA gain, –60-dB input signal, master mode at SE input.
What does -60dB input means…
Hi,
Welcome to E2E, Thanks for your interest in our products!.
The process you are following is correct, the issue is that there is an error in the datasheet, the address of the SIGDET_LOSS_TIME register is actually 0x33, not 0x34. Sorry for the confusion…
Part Number: PCM1862-Q1 Other Parts Discussed in Thread: PCM1862 , PCM1860 Hello.
I am trying to desing a audio card to use with pine64 ( www.pine64.org/
I am thinking to use PCM1862-Q1 IC( www.ti.com/.../pcm1865-q1.pdf schematic on page 23).
I…
Other Parts Discussed in Thread: PCM1865 , PCM1863 Hi,
I have questions about 'Audio Data Interface Timing' of PCM1863 and PCM1865.
Q1. According to figure 45, the minimum LRCK Period (tLRCP) is 10 microseconds, this value means the maximum sample…
Hi KISO-san,
Thank you for catching the contradictory statements.
Q1 & Q2
Kazuki KISO said: >The pulse width of the interrupt signal can be changed between 1ms, 2ms, 3ms and 4ms. >The interrupt controlled cannot remain asserted , the status bits…
Part Number: PCM6360-Q1 Other Parts Discussed in Thread: PCM1865
Hi,
Here we have a project designed in with PCM6360Q1 which has built in PGA besides digital volume control. We need a sensitivity range from 7V to 200mV with this project. But when…
Part Number: PCM6240-Q1 Other Parts Discussed in Thread: PCM1865 Hi Team,
We are trying to use PCM6240-Q1 in our new design in place of PCM1865. The data sheet says that on I2S bus, we can have 64 slots (channels). Here we got confusion, whether we…