Part Number: PCM2707EVM-U Greetings,
I would like to determine if the I2S bit clock ( BCK ) signal generated by this part is continuous or discontinuous ( burst ).
Thanks and rgds, David
Part Number: PCM1794A Other Parts Discussed in Thread: DIR9001 , , SN74LVC157A Hi, is it possible to simply share I2S bus between DIR9001 and PCM1794A with resistors in the path, or is it necessary to use multiplexer? In case of multiplexer, which part…
Hi, Arash
I reattach the photos. I added the 'HOST' Pin of PCM2707 to the waveform.
In my device, the PCM2707 is connected to a USB 2.0 hub(FE1.1S). The hub controls power of the UFP devices in Ganged Mode. I designed that this signal controls…
Part Number: PCM2707
Hi Team, Cusotmer is evaluating the PCM2705/5 USB codec. Customer has questiona as below.
"How many sampling rates can be supported by USB input in PCM270XC?"
I am not sure the relation between USB sides' sampling rate.…
Part Number: PCM2707 Hi, standard typical circuit connection for PCM2706 or PCM2707 is with headphone support (pdf page 30). Device have decoupling capacitors C3, C4 for VCCR and VCCL (supply for headphone amplifier) - with both, bus powered and self…
Part Number: PCM2707 Before committing to more elaborate designs, I'm trying to give it a quick try. In particular, I want to see if there are any surprises with Linux recognizing the device (mostly interested in Ubuntu).
If I want to start by just…
Part Number: PCM2707
Hello,
A while ago I attempted a very crude minimal test circuit that didn't work --- it was missing decoupling capacitors and possibly some other important connections.
I tried this time something close to the circuit in Fig…